Connected Intelligent LED Lighting Networks: Intelligent Lighting Integrated Within
Smart Buildings
By Paul Golata, Mouser Electronics
Today’s LED lighting does much more than illuminate otherwise dark spaces. When combined with low voltage
IP-based infrastructure in a connected intelligent network, LED lighting becomes part of a powerful network of
systems that work cooperatively to collect, analyze, manage, control, and respond to set objectives and real-time
sensor feedback. The resulting “smart building” is more holistic in its operational performance
because it can dynamically respond to operating issues, thereby increasing efficiency and saving both power and
costs.
How does integrated intelligent lighting work with other systems? And what technologies are needed to integrate
systems and maximize benefits? This article explores connected intelligent lighting and discusses infrastructure
technologies.
Intelligent LED Lighting Networks
The basic premise behind connected intelligent LED networks is to have lighting control go from a centralized and
relatively universal approach across a large area of the building space and to change it over to a solution
that’s tailored to the specific needs of smaller segments within the building. What’s more, because
the lighting is part of an intelligent network, the lighting integrates with—and can respond to—other
components on the network. This is especially valuable in commercial office buildings, healthcare facilities,
warehouses, manufacturing and industrial facilities, and similar large or multipurpose spaces where a
one-size-fits-all approach is ineffective or inefficient.
Imagine a building that’s controlled through automated heating, ventilation, and air conditioning (HVAC).
The HVAC monitors and adjusts the temperature to make the surroundings suitable for human comfort and machine
performance, as well as optimal efficiencies and cost. A connected intelligent LED lighting network would allow
lighting to be synchronized into these same set of objectives. This actively couples lighting response with
environmental climate control. As a result, connected intelligent lighting networks increase the ability for the
network users to adjust light to increase human productivity, positive mood, concentration, and well-being. It can
respond to potential advantages achieved by adjusting light in synchronization with the natural human circadian
cycle and additionally by reducing or increasing the required light depending on the amount of sunlight coming
through external windows.
LED Lighting and PoE
The key technology behind intelligent LED lighting networks is Power over Internet (PoE), which brings the
low-voltage cabling and equipment that connect Internet of Things (IoT) assets to LED fixtures. PoE is simple and
available because of the success of IP-based infrastructure platforms. By using PoE as the artery of the LED
lighting power and control system, lighting is incorporated into the building as an IoT asset. Besides the
tremendous advantage of providing power and data over a single-layer infrastructure, PoE is also less costly than
copper cable. As Figure 1 shows, PoE system architecture includes the following devices, discussed in the
next sections:
- PoE gateways
- LED light fixtures
- LED lights
- LED smart drivers
- LED cable harnesses
- Sensors
- Wireless switches and dimmers
Figure 1: PoE system architecture includes gateways, fixtures, lights,
drivers, cable harnesses, sensors, and wireless switches and dimmers. (Source: Molex Transcend® Network
Connected Lighting)
PoE Gateways
While computers and network interfaces control the management layer of the PoE network, the start of any integrated
LED lighting system relies greatly on the device layer and the level of system components used to make the network.
A PoE gateway is the device at the heart of the system. These gateways connect to, control, and power the light
fixture luminaries that operate the LEDs. They are able to control LED lighting functions, including dimming, color
tuning, and sensor reporting. These gateways are capable of delivering up to 60W. In cases where more wattage is
needed, such as in high bay lighting, AC line voltage (120VAC–277VAC) is still
required, wherein the devices can be controlled by a wireless line voltage relay.
In the IP industry, the standards derived from the Advanced Telecommunications Computing Architecture (ATCA or
AdvancedTCA) call out for 48VDC. Because of this standard, it is natural to provide POE gateways that are
configured to one of the following configurations:
- Unregulated 48VDC
- Constant voltage 24VDC/48VDC
- Constant current
Wireless PoE gateways that conform to IEEE 802 standards may also be used. They run at standard frequencies
(902MHz, North America; 868MHz, Europe). Commonly, they have an effective range of about 15m. They enable secure
two-way communication for control status of multiple wireless devices without designers needing to have cause for
concern with interference happening with other devices.
LED Light Fixtures
The LED light fixture itself is a critical and enabling component of the system. At its core, the fixture relies on
the selection of the specific illuminating LED itself. In LED lighting systems that are not intelligently connected
and networked, the LEDs used are substituted for traditional lights. The inherent superior technological
efficiencies of LEDs relative to incandescent or fluorescent lights provide the efficiency benefits. However,
connected intelligent lighting systems ratchet the whole system up a level. They take and add PoE gateways, lighting
control sensors, and advanced network-managed software systems to provide a total environment that adds significant
feedback and control into the system. This enhancement makes the light themselves human centric and capable of being
controlled based upon data, analysis, and decision criteria of the network user.
LED Lights
LED manufactures are constantly improving LEDs by increasing their efficacy (lm/W) and reducing the cost per lumen
($/lm). Examples of LED manufactures that provide excellent products for light fixture manufactures abound:
- Cree, a leader in illumination LEDs created the XLAMP XHP70.2 Extreme High Power LED, which deliver low system cost
through high lumen density, reliability, and color consistency. Improvements in lumen density, voltage
characteristics, reliability, and optical performance in a 7.0mm x 7.0mm package.
- Lumileds has developed the LUXEON MX
LED Module which is a high-power, multi-die emitter, enabling cost-effective, high-reliability fixtures for
High Bay and Outdoor applications. It boasts up to 150lm/W efficacy in a 12VDC configuration to produce
up to 1,200 lumens at 85°C.
- OSRAM Opto Semiconductors makes the DURIS E
2835 LED, which combines good efficacy and a wide viewing angle into a compact 2.8mm x 3.5mm Plastic Leaded
Chip Carrier (PLCC) package. These surface-mount LEDs are available with a Correlated Color Temperature (CCT) of
2700K to 6500K.
Additional useful products include these:
- Surge protectors: Littelfuse manufactures the PLED6N Open LED Protector, which provides a switching electronic
shunt path when an LED in an LED string fails as an open circuit. Its low height profile (1.1mm) makes it
compatible with 1W rated LEDs with a nominal 350mA current at 3VDC (1W).
- Connectors: Molex brings connector innovation forward with the Molex Lite-TrapTM and Mini Lite-TrapTM
SMT Wire-to-Board Connector System, Push-Button Type. These offer profile heights down to 2.65mm, easy wire
removal, low wire insertion, and high wire retention forces for thin LED lighting-module applications. Its
ultra-thin profile prevents shadowing in LED lighting applications.
- LED drivers: Texas Instruments makes the TPS92515/TPS92515-Q1 2A LED drivers, which provide
compact monolithic switching regulators integrating a low resistance N-Channel MOSFET. Intended for
high-brightness LED lighting applications where efficiency, high bandwidth, PWM and/or analog dimming are
important. Infineon is a global leader in MOSFETs. Additionally, Infineon
provides the CoolMOS® CE whereby
its excellent efficiency, ease-of-use, and EMI performance at an attractive cost make the series the product of
choice for LED drivers or LED tubes. They can be applied in buck, flyback, PFC, and LLC topology.
Smart LED Drivers
Intelligent LED drivers supply the appropriate power and conditioning signals for the LED engine. After receiving
control data and power from the PoE gateway, the LED driver can respond to information and drive tasks based upon a
coordinated design, control, and management system emanating from the connected network. At present, they are
available in single-channel or dual-channel configurations capable of driving LED lighting fixtures with constant
currents at output voltages of 12VDC-42VDC and a maximum output power of 45W. They can be
daisy-chained together so that that up to eight devices can be driven from a single PoE gateway.
LED Cable Harnesses
LED cable harnesses are not yet standard as a means of connecting smart LED drivers in order to provide the low
voltage power distribution and data communication necessary to control LED lighting fixtures, sensors, and
actuators. An excellent way to design and do so until these LED cable harnesses become industry standard is using
Molex’s excellent solution for this application: Their new Micro-Fit 3.0 Interconnect System (Figure
2). This system is designed to meet the need for a high contact density signal or power connector. They
are built with a miniature 3.00mm (0.118”) pitch, yet they retain many of the features found on larger power
connectors and can carry up to 5.0A of current. These connectors are proven in their reliability, durability, and
ease of use.
Figure 2: The Molex Micro-Fit™ 3.0 Interconnect System is reliable,
durable, and easy to use. (Source: Mouser
Electronics)
Sensors
Sensors are a necessary part of the control loop in order to enable the digital building. Sensors can be either
wireless or wired, and they can be deployed and powered though the PoE gateway or integrated into the LED lighting
fixture.
Wireless ambient light sensors are a commonly deployed device in this arrangement. They are self-powered through
collecting light and performing energy harvesting, which makes them
economical and reliable. They are capable of measuring and reporting to a central host the level of available
natural light allowing the network to make real-time adjustments and decisions.
Other common types of sensors used in LED lighting networks include: Air quality, color temperature, humidity,
passive infrared (PIR) motion/presence, on/off, proximity, power, and temperature.
Wireless Switches & Dimmers
Self-powered wireless wall switches and dimmers employ energy harvesting technology to communicate wirelessly with
the PoE gateway, providing convenient control of lighting, temperature, and miscellaneous electric loads. The local
switch/dimmer pads are self-powered and never require batteries because the simple act of pressing the rocker
generates enough energy to send a wireless signal to gateway devices.
Conclusion
Intelligent and networked LED lighting systems are forming new ways to apply LED lighting in the world of smart
buildings and information technology. These lighting systems require a variety of technologies, including gateways,
fixtures, lights, smart drivers, cable harnesses, sensors, and wireless switches and dimmers. The future is bright
as system-level intelligence converges with our working environments, enabling the smart building of tomorrow today.
Paul Golata joined Mouser Electronics in 2011. As a Senior Technical Content Specialist, Paul is accountable for
contributing to the strategic leadership, tactical execution, and overall product line marketing direction for
advanced technology related products. Paul provides design engineers with the newest and latest information
delivered through the creation of unique and valuable technical content that facilitates and enhances Mouser
Electronics as the preferred distributor of choice.
Before Mouser Electronics, he served in various manufacturing, marketing, and sales related
roles for Arrow Electronics, JDSU, Balzers Optics, Piper Jaffray, Melles Griot, and Hughes Aircraft Company. Paul
holds a BSEET from DeVry Institute of Technology—Chicago, IL; an MBA from Pepperdine
University—Malibu, CA; an MDiv w/BL from Southwestern Baptist Theological Seminary—Fort Worth, TX; and
a PhD from Southwestern Baptist Theological Seminary—Fort Worth, TX.