A voltage regulator takes as an input an unregulated source of voltage and current and
outputs a fixed, stable voltage at the required power. The voltage regulator is designed to
maintain a stable output voltage regardless of any changes to the input voltage or load
conditions. The specifications of a voltage regulator state how much the input voltage can
vary, and the conditions under which it can maintain the output voltage and power under
load.
Linear Voltage Regulators
Linear voltage regulators are three-terminal ICs that smooth the rectified AC signal into a
nice, stable DC output. In linear regulated power supplies almost all the excess power is
dissipated as waste heat. This heat must be taken into account in the design of the power
supply and can require air vents in the power supply housings, and sometimes a fan. With
very low ripple and high reliability, linear regulated power supplies are optimal for
sensitive low power electronic equipment.
A linear voltage regulator is selected by matching the available input voltage and power to
the required output voltage and power. Usually the required output voltage is fixed and has
a specified maximum output current. The regulator must be able to handle a variable or
unstable input voltage at a specific power rating.
Low Dropout Regulators
Low Dropout Voltage Regulators (LDO) are a type of linear voltage regulator with a noticeably
low quiescent current and very low voltage loss. LDOs require less headroom, or dropout
voltage, to maintain a regulated output voltage. Dropout voltage is the minimum voltage
potential needed across the regulator to keep working well. For digital circuits, low
dropout regulators must be efficient and be able to handle rapidly changing demands for
output currents. This is especially true in power-sensitive microcontroller-based systems
where the microcontroller may turn peripherals on and off, change clock speed, and enter or
leave different low power modes. An LDO must handle these rapidly changing current
requirements with no lag.
While all voltage regulators can have some noise on the output voltage on the order of
millivolts, LDOs have higher noise than standard linear voltage regulators. In general, the
lower the dropout voltage, the higher the output noise.