Mouser Now Shipping New Vishay Semiconductors VEML6046X00 Color Sensor for Automotive Applications

New Product Announcement

Connect With Us


Learn more about the VEML6046X00 color sensor
Learn more about the VEML6046X00 color sensor

July 30, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new VEML6046X00 color sensor from Vishay Semiconductors. The VEML6046X00 is the industry's first automotive-qualified, surface-mount, high-accuracy 16-bit, RGBIR color sensor with an I2C interface. This device is ideal for display backlight controls, infotainment systems, rear-view mirror dimming, lighting control systems, and color recognition in automotive applications.

The Vishay Semiconductors VEML6046X00 color sensor, available from Mouser, features highly sensitive photodiodes, a low-noise amplifier, and a 16-bit A/D converter that supports an easy-to-use I2C bus communication interface and additional interrupt features. With separate red, green, blue, and infrared (IR) channels, the VEML6046X00 sensor allows for the calculation of the color temperature to enable white point balancing for displays in an automotive-grade device that is RoHS compliant and halogen-free and available in a miniature, low profile, opaque, surface-mount package (2.67 × 2.45 × 0.6 mm3 (L × W × H), operating at a 2.5 to 3.6-volt supply voltage range.

The human eye-like spectral sensitivity of the VEML6046X00's green channel ensures highly accurate measurements, while the IR channel facilitates a stable output over a wide range of light sources. With an ambient light range from 0 lx to 176 klx, the sensor will not saturate in daylight, while its high sensitivity of 0.0053 lx/ct allows the device to be placed behind dark cover glass.

Also available from Mouser is the Vishay Semiconductors VEML6046X00-SB sensor board, a compact and versatile evaluation platform designed to demonstrate the capabilities of the VEML6046X00 high-accuracy color sensor. The VEML6046X00-SB board is designed to work with the Vishay SensorXplorer, which enables connection to the USB port of a PC.

To learn more about the VEML6046X00 color sensor, visit: https://www.mouser.com/new/vishay/vishay-veml6046x00-color-sensor/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Vishay Semiconductors

2026 - Vishay Intertechnology manufactures several kinds of discrete semiconductors. These typically perform a single function, such as switching, amplifying, rectifying, or transmitting electrical signals. Vishay Intertechnology also manufactures selected ICs, which combine the functions of multiple components on a single chip, as well as modules, which include multiple components in a single package. Vishay Intertechnology’s semiconductors portfolio includes MOSFETs (low-voltage, medium-voltage, and high-voltage), ICs (both power and analog), a wide range of diodes and rectifiers, and many different types of optoelectronic products. The Company is a market and technology leader in power rectifiers, low-voltage power MOSFETs, and infrared components.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764