Fluke Solmetric PVA-1500 PV Analyzer I-V Curve Trace Kit for Performance Verification in PV Solar Arrays, Now at Mouser

New Product Announcement

Connect With Us


July 23, 2024Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is now stocking the Solmetric PVA-1500 PV analyzer I-V curve trace kit from Fluke Corporation. Taking on a more efficient approach instead of combining traditional digital multimeters, clamp meters and irradiance meters to measure the I-V (current versus voltage) curve of a photovoltaic (PV) string or module using a capacitive load, the PVA-1500 combines all those metering options into one cutting-edge solution that more reliably assesses the health and performance of PV solar modules, strings and arrays. The PVA-1500 enables the accurate measurement and verification of an I-V curve so technicians can immediately evaluate the solar panels' health, detect any degradation in power, or identify issues such as shading, damage or faulty components.

The PVA-1500 PV analyzer I-V curve trace kit, available from Mouser Electronics, can deliver quick and detailed performance data checking via its intuitive user interface by accurately measuring and displaying high throughput I-V curve tracing up to 1500V and 30A at the string level by connecting directly to the string or at a combiner box. The I-V curve trace points can be selected at 100 or 500. The PVA-1500 then generates the P-V (power versus voltage) curve, Isc, Voc, Imp, Vmp, Pmax, fill factor and performance factor to enable an immediate analysis of curve datasets to detect outliers and use the stored data as a baseline for future performance evaluations. To address some testing challenges with high-efficiency PV modules with higher capacitance (>19% module efficiency), Fluke offers the PVA-1500HE2, also available for purchase on the Mouser website. This kit option measures all string types up to 30 amps, operates with an exceptional swift sweep-to-sweep delay of 9 seconds (at Voc<1350V), and is designed to measure 3.5 MW within an hour and withstand the inrush current of higher temperature environments all day without overheating.

The PVA-1500 can communicate wirelessly with a PC via Wi-Fi with a line-of-sight wireless range of 100m, offering faster setup and mobility with the flexibility to measure multiple combiner boxes on a single SolSensor setup. The PVA-1500 kits are "in-the-field firmware update-ready" and offer a database of over 70,000 modules with automatic updates. In addition, the kits are supported by a free downloadable Data Analysis Tool (DAT) that validates the captured data results in the field and streamlines the PVA I-V curve data analysis into multiple formats.

To learn more, visit https://www.mouser.com/new/fluke/fluke-solmetric-pva-1500/.

 

As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Fluke

2026 - Fluke Corporation is a world leader in electronic test tools and software. Since 1948, Fluke has been at the forefront of innovation, delivering reliable, easy-to-use solutions that have become essential in manufacturing, industrial maintenance, and service environments.

From installing and maintaining complex electrical systems to performing precision measurements and ensuring quality control, Fluke tools help keep critical operations running smoothly across the globe. Built for portability, durability, and safety, Fluke products are trusted by professionals who demand performance and accuracy—every time.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764