South Africa - Flag South Africa

Incoterms:DDU
Duty, customs fees and taxes are collected at time of delivery.

Please confirm your currency selection:

US Dollars
Free shipping on most orders over $150 (USD)
All major credit cards accepted

Euros
Free shipping on most orders over 150 € (EUR)
All major credit cards accepted

South African Rand
Free shipping on most orders over R2 000 (ZAR)
American Express not accepted as a method of payment

British Pounds
Free shipping on most orders over £150 (GBP)
All major credit cards accepted

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


From Roomba to Rosie: Getting Closer To the Chore-Free Home of the Future Justin Risedorf
Current household robots are largely one trick ponies. Sure it’s nice to have a dog bowl on wheels quietly move around the room, sucking up whatever the kids brought in on their shoes, but what else can it do? The market is flooded with robots that can vacuum the carpet, mow the lawn or remember to water your plants. Recently, I came across a robot to change your cat litter which would be useless… unless you made the mistake of owning a cat in the first place. Relax… I’m kidding! But I know what you’re thinking, “How long until I get to turn on a humanoid protocol droid that can handle complex tasks, speak my language, and help out around the ole’ moisture farm?” The good news is, sooner than you thought.

Home Automation – In the Beginning and Beyond! Rudy Ramos
Home automation has come a long way since The Clapper was first introduced back in 1986. Today you can find a plethora of home automation products to augment all of the creature comforts already found in most American homes.

From Rosie to JARVIS Grant Imahara
When I was a kid, I used to watch a cartoon called “The Jetsons”, which was set in a future where flying cars fold up into suitcases, a dinner table automatically clears away the dishes (by smashing them and sweeping them up), and sassy robotic maids do all the housework. Although I’m still waiting for my flying car, some of today’s automation technologies are a lot closer to the future world of The Jetsons than you might think.

"The Chip" David Fambrough
Since the beginning of time, man has looked up to the stars and wondered…how can we get there? We did get there, in the summer of 1969 when astronaut Neil Armstrong made one giant leap for mankind. NONE of this would have been possible without the development of both fast and small electronic components that now form the backbone of information and processing technology.

Weird RF Part 3: Communication with Submerged Subs Barry Manz
There is no shortage of stories about bizarre Department of Defense programs, but this one is surely in the top tier. Extremely Low Frequency (ELF) signal propagation (we’re talking 3 to 30Hz) allows signals to pass through the earth and throughout the oceans to depths of several hundred feet, allowing a system at a single location to communicate nearly anywhere on the planet. This made it rather appealing for communicating with submerged submarines and might be able to function in the event of a nuclear strike. The idea was championed not just by the U.S., but by the Soviet Union and India as well. Signals degrade rapidly in the ocean, so when a submarine is submerged, it is less likely to receive communication. The purpose of Elf was to reach deeply submerged subs sufficiently to let them know to surface to receive communications through normal (and better) radio communications.

Lexus Builds Hoverboard Because Hoverboard Erik Smith
People seem to just want to keep toying with my hoverboard-yearning heart. After Funny or Die's almost convincing, but ultimate hoax, and Hendo Hover's exorbitantly priced Kickstarter campaign, Lexus is now in on the hover-game. Earlier today, the luxury car manufacturer released a teaser video, claiming to have created a "real, rideable hoverboard."

5 Tips for Getting Started In Electronics Mike Parks
Electronics is an amazing profession and hobby. The notion that one can harness the forces of nature and bend them to one’s whim is immensely satisfying. With the resurgence of the DIY spirit and the evolution of the Maker Movement, getting started in electronics has never been easier. Embedded open source platforms such as Arduino and BeagleBone provide a fantastic jumping in point for learning electronics and software. I could only have dreamt of the resources we have today when I was first starting out. With that in mind, here are my five tips for getting started in electronics based on what I’ve learned over the last 20 years.

Internet of Stuff Arden Henderson
The big buzzphrase today is The Internet of Things (IoT). Things that connect to the internet. Connected stuff. Lots of stuff. And the products that connect to the internet are rolling out at ever increasing rates. Connected cars, connected homes, connected things in homes, connected houses, connected wearables, connected stores for shopping, connected restaurants for dining, connected roads and bridges, and on and on. Hotel robots. Smart stuff. What stuff will be connected? The better question is what will not be connected. Rocks, for example. Wait, someone will market a rock monitor, connected to the internet by forest wifi. When a rock rolls in a forest, does it make a sound?

Connected Contact Lenses Justin Risedorf
Today, we are a long way from the initial offerings of contact lens technology. Research has taken the industry from small, hard plastic lenses that required a constant flow of lubricating drops (and could pop out when a person blinks), to soft lenses that make it easier for the eye to breathe while being worn.

Space, The Harshest Frontier David Fambrough
What makes for a harsh environment? For a person, that’s an inhospitable set of conditions that can cause bodily harm over a period of time. Space is one of the harshest environments you can imagine for human beings – even without monstrous alien predators. Pressure, or the lack of it, temperature, or the lack of it, high-energy particles, and radiation are just not very human-friendly. It’s a cold, dark place that lacks many of the creature comforts of home – like water and air.

All Authors

Show More Show More
View Blogs by Date

Archives